IP.DEFAULTINTERFACE

Description

This keyword sets the default TCP/IP interface to use. Allowed interfaces are either the Service Interface or EthernetOverEtherCAT (EoE). This is only necessary when a host using WB or other custom IDEs (like PuTTY) attempt to connect to the drive from an IP address that is not in the drive subnet (as set either using IP.SUBNET or using TwinCAT). It is not needed when the host and drive are on the same subnet as seen by the drive.

Examples

Usage

Use this keyword to choose the right interface when the host is trying to connect to the drive from an IP address that is not in the drive’s subnet for that interface.

The default interface is the Service Interface. The code below shows how to set the default interface to the EoE interface and then show the keyword help.

Code

-->IP.DEFAULTINTERFACE 1

-->DRV.HELP IP.DEFAULTINTERFACE

Help for: IP.DEFAULTINTERFACE [Integer] [NV] [ReadWrite] [Enum]

Minval = 0

Maxval = 1

Default = 0

Actual value = 1 (Default to EoE)

Values = 0 (Default to Service Interface), 1 (Default to EoE)

Context

For more information on IP configuration, see Finding and Connecting to a Device. For more information on EoE, see Setting up Ethernet over EtherCAT (EOE).

Versions

Action Version Notes
Implemented 02-04-00-000

 

General Information

Type Read/Write
Units N/A
Range 0 to 1
Default Value 0
Data Type Integer
See Also

 

Stored in Non Volatile Memory

Yes

Variants Supported

All variants supported.

Fieldbus Information

EtherCAT CoE and CANopen

Command

Index

SubIndex

Data Type

Units

Float Scale

Access

PDO Mappable

IP.DEFAULTINTERFACE

3013h

02h

Unsigned8

-

-

Read/Write

No

IP.DEFAULTINTERFACE

4200h

00h

Unsigned8

-

-

Read/Write

No

EtherNet/IP

Name

ID

Hex

Data Type

Access

Units

IP.DEFAULTINTERFACE

2200

898

Unsigned8

Read/Write

-

PROFINET

Parameter

PNU

Data Type

Access

Units

IP.DEFAULTINTERFACE

2200

Unsigned8

Read/Write

-